Hi,
I tested writing CSM settings to OTP on a F28377S using the flash API Fapi_issueProgrammingCommand function with flag Fapi_DataOnly. Now, if I cycle the power, the DSP gets stuck in boot rom with a NMI RAM unrecoverable error -> Address : 0x3FE444.
Do I have this error because I used DataOnly flag when writing to OTP flash memory? During bootup ECC detects an error and hangs there? Is there another possible cause for this? Are there other registers I can check to give you more information on the DSP status?
Any help will be appreciated.
Regards,