This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Respected Sir,
I'm unable to display the adc values on the simulink scpoe with RTDX as i'm new to the simulink and ccs environment. after surfing for help I tried to find a command called
>> rtdxtutorial
but when i tried to excute in the matlab window
below are the errors I observed
>> rtdxtutorial
==================================================================
The RTDXTUTORIAL is an example script intended to get the user
started with the RTDX.
A simple target DSP application is loaded and run on the target
DSP, and data messages are transferred via RTDX between the host
application (MATLAB) and the target DSP. The tutorial writes
integers 1:10 to the target DSP. The target DSP takes the array
of integers, increments it by 1, and writes the resultant array
to the host. This action is performed 20 successive times, with
each iteration incrementing the previous array result by one.
The 20 messages are read using various output formats.
==================================================================
Error using Link.ccssetup/Connect
Cannot start CCS application (COM error ID: 0x80040154).
Verify that your CCS software is installed and configured
properly.
Error in ccsboardinfo (line 68)
ccssetup.Connect(); % Connect to CCS Setup
Error in getNumTargetsInCcsSetup (line 7)
setupinfo = ccsboardinfo;
Error in selectBoardProcNumbers (line 13)
numTargets = getNumTargetsInCcsSetup;
Error in rtdxtutorial (line 42)
[boardNum,procNum] = selectBoardProcNumbers;
so how can i correct the very starting error (COM error ID: 0x80040154) as it say LINKCCSSETUP error, is their any linking file missing and the ccs version i'm using is
CCSv6.1.1.00022
Regards,
Anuroop