Other Parts Discussed in Thread: TMS320F28335
Dear all,
I am currently using in my project the TMS320F28335, however, it is currently running out of RAM memory (68K) to store the program. I was considering the option of upgrading to a more powerful DSC with more RAM memory (and possibly other advantages), however, since the project is quite in an advanced situation, I would like this other DSC to be as much compatible as possible (in the ideal case, just replacing the chip).
Thus, do you know if there is a 100% compatible DSC with the F28335 ?? In case there isn't, which one would be the 'most compatible' one and what are the most important changes I would have to do?
To give more information, i'm using the 176 pin version of the F28335, and I saw that the F2837X family has also that possibility, however, the more similar the pin distribution is, the better it would be (ideally the same, of course).
Best regards,
Jorge.