This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2Prog via SCI-A using the F28335 controlCARD Release 2.2 Sector Violation...

Hi,

Getting a "Sector Violation" when I try to program the F28335 over a Serial Line.  I suspect the hex file is being generated incorrectly...

The application is basically the Example_2823xAdcToDMA project with a few additions made by myself.  The Memory Map is as shown here:

There is no Flash component as I use the 28335_RAM_lnk.cmd file.  The code is fine as I can program using the JTAG (XDS200) and I can see output via RealTerm when the code runs (I output "Hello World!"), so I know the Serial Comms is good.

I have tried generating the .hex file as per the c2prog manual:

hex2000 -romwidth 16 -memwidth 16 -i -o output.hex Example_2823xAdcToDMA.out  -------> (1)

And I have also tried using (what I think is correct) the following via CCS:

hex2000 --boot --sci8 --intel ---------->(2)

And finally, I have tried:

hex2000 --sci8 --intel ---------->(3)

The c2prog settings are as per the attached diagram.

The Experimenter board has the correct bootmode settings (0-1-1-1) on SW2 and SW1 is set to 0.

The following are the Sector Violations I receive when I try to program over the Serial Port:

(1)---------------> Sector Violation 0x95C0...0x95CF

(2)---------------> Sector Violation 0x320...0x32F

(3)---------------> Sector Violation 0x10180...0x1018F

It sounds like I don't have a valid set of mappings in the hex file or I have an incorrect processor selected in c2prog.  Can anyone advise on what I need to check for in order to get this working?

Many thanks,

Mike.