This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35 (FCC) not working with g3_dc_AM335X_aes_msb_loadng.exe

Hello

Our setup contains a F28M35 pair.
If I intialize both with ZeroConf, they are finding each other.
If I initalize the DC with ZeroConf our SN is joining.
But If I start g3_dc_AM335X_aes_msb_loadng.exe on the DC device there is a "no beacon" error on the SNs discovery step.

./g3_dc_AM335X_aes_msb_loadng.exe -c /dev/ttyUSB1 -B tonemask_fcc2 -F 1
#########################################################################
################# G3 Data Concentrator Version 4.7.0.6 ##############
#########################################################################
Original System Information from device ...

*** SYSTEM INFORMATION ***
Firmware Version.................... 7.6.5.10
Device Type......................... G3
Device Mode......................... MAC
Hardware Revision................... pre Rev. D
Host Port........................... SCI-A
Diag Port........................... SCI-B
Apply RPY........................... no
Auto Mode........................... no
G3 Address Type..................... 0
G3 Long Address..................... ffeeddccbbaa9988
G3 Short Address.................... 0
G3 MAC Segment Length............... 0

DEV_shutDown_Handler: SHUT_DOWN returned success.
Pausing to allow device to reset.
DEV_setSysConfig_Handler: LOAD_SYSTEM_CONFIG returned success.
System Information of device has been set to...

*** SYSTEM INFORMATION ***
Firmware Version.................... 7.6.5.10
Device Type......................... G3
Device Mode......................... MAC
Hardware Revision................... pre Rev. D
Host Port........................... SCI-A
Diag Port........................... SCI-B
Apply RPY........................... no
Auto Mode........................... no
G3 Address Type..................... 0
G3 Long Address..................... ffeeddccbbaa9988
G3 Short Address.................... 0xffff
G3 MAC Segment Length............... 0

The tonemask_fcc2 file contains (fcc full band):
0x21 0x48 0xff 0xff 0xff 0xff 0xff 0xff 0xff 0xff 0xff 0x00 0x00 0x00

A suspect field is G3 Short Address:0xFFFF.
Further the start-net command is blocking on the g3_mgmt_cli_AM335X

Have you any idea what could be wrong here?

Thanks

Roman