Hello,
I'm using a TMS320F28075 and am triggering an ADC SOC using a GPIO configured as a digital input and ADCEXTSOC via Input X-Bar INPUT5. It's triggering the SOC every rising edge of the GPIO -- however, the signal on the GPIO is a square wave and I need to trigger SOCs on both the rising and falling edges. So far I haven't found a direct way of triggering an SOC based on the falling edge, too .... it seems like maybe I could route the same GPIO to the ePWM X-bar and try to sync an ePWM and somehow generate another SOC based off that PWM... but I'd rather not waste an ePWM and I'm wondering if there's a more straightforward way that I'm missing? I also just started looking at routing the Input X-Bar to the Digital Compare Submodule to see if this is something I can use for this in conjunction with the Event-Trigger submodule, instead... Any direction would be appreciated.
Thanks,
Dave