Other Parts Discussed in Thread: CONTROLSUITE
Dears
I have a F28377S Launchpad, but I find that in controlSUITE(ver 3.4.0), the USB peripheral demo code for Delfino F2837xS is not compatible with the Launchpad. In demo code, the monitor UART is {GPIO28,GPIO29}, but on the Launchpad board, F2232H is connected to {GPIO84,GPIO85}; In demo code, the USB driver will check the status of VBUS, PFLT, EPEN, and ID, but there no such supporting hardware on the Launchpad. It seems that the demo code is more suitable for F28377D controlCARD.
Then my question is: where can I find USB demo code for F28377S Launchpad? Thanks