Other Parts Discussed in Thread: TMS320F28377D
I am working through the F2837xD workshop Guide. The first Lab is to blink two LEDe, each controlled by a different processor. CCS will not let me add files to the project for CPU2. The code will blink the LED using CPU1. When looking at the Project Explorer window, the Include files for Lab1_cpu01 are listed and used ok during the build of the code. Two of the three Include files for Lab1_cpu02 are listed, but grayed-out. When I us "Add Files" to add the files to Lab1_cpu02 a window pups up with the message: "Could not add:" then it list the files I am trying to add.