Dear all
Have had a lot of issues regarding the 2nd 28335 Delfino control card that I had purchased in compensation to the first one that got 'burnt' mysteriously as a part of a 1-phase grid-connected inverter project. Yes I admit it may have been a spike while connecting 5 of the analog inuts in a closed loop configuration although we had used op-amp 741 scaling circuits to ensure 3 V range but the error seemed to be something different. Now the new one worked well for 2 weeks and we managed to complete our grid-connected inverter but when we ran it after 2 days of inactivity, it failed to load the Simulink compiled programs. The next day it failed to connect--Emulator XDS100 USB error---as before. A week later, it gets connected but now says "ADC Calibration error, check if evice is unlocked and re-calibrate". The program also gets loaded but while running it says "Data verification failed at address 0 8000. Please verify target memory and memory map". To be clear, I am just using Simulink blocks to compile the controller block models and loading it to target via CCS V3.3 I have had no exposure to CCS coding.
Regards