This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC conversion of an external square wave

Hi all,

I'm using TMS320C2000 Experimental kit with F28335

I generated two square waves using 555 and it looks very nice at Scope. One signal is 6msec period, second signal is 1.5msec period.

My ADC configuration is as follows:

//ADC parameters
#define ADC_MODCLK 0x3                                 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3)   = 25.0 MHz
#define ADC_CKPS   0x1                                     // Options 0 to F. ADC module clock = HSPCLK/2*ADC_CKPS = 25.0MHz/(1*2) = 12.5MHz
#define ADC_SHCLK  0x1                                   // S/H width in ADC module periods                        = 2 ADC clocks

SysCtrlRegs.HISPCP.all = ADC_MODCLK;

AdcRegs.ADCTRL1.bit.ACQ_PS = ADC_SHCLK;     // sampling window

AdcRegs.ADCTRL3.bit.ADCCLKPS = ADC_CKPS;

AdcRegs.ADCTRL1.bit.CPS = 0;                // divide by 1 the FCLK Options 0 (divide by 1) or 1 (divide by 2)

AdcRegs.ADCTRL3.bit.SMODE_SEL = 1; //Simultaneous mode to convert 2 signals in parallel

First question is what will be the sampling rate?

I saw the following comment in one of the examples:

//If Simultaneous mode enabled: Sample rate = 1/[(3+ACQ_PS)*ADC clock in ns]

According to this teh sampling rate is: 1/[4*80nsec] = 3.125MHz -->0.32usec - should be enough for my signals

Using the graph feature I see the following:

Signal 6msec

Signal 1.5msec:

Why is this so inaccurate? Where is the problem?

Thanks