I have a mature product that is in the field for 3+ years. It uses a 28335 micro on a custom board. Recently there has been a problem on power up where the processor does not run. Powering down the board brings the processor back to life.The board design has not changed. When I try to connect with a XDS510 emulator I get this error:
This project NEVER intentionally goes into low power mode.
If I press YES the processor comes to life.
Which register does CCS use to determine that the processor is in low power mode?
How does it bring it out of low power mode?
Any idea what could be causing the processor to enter low power mode?