Hi Dear Masters,
I try to get message canbus line with TMS320F28054F
I use as a reference project "Example_2805xECanBack2Back"
I am sure, I can transmit canbus message successfully. (I see message which i send via another custom design board)
But i cannot receive message with same canbus baud rate
I look at "Error and Status Register (CANES) Field"
RM (Receive Mode) bit generally 1
BE (Bit Error Flag) bit always 1
When BE bit is 1, CANBUS reference guide say that : "The received bit does not match the transmitted bit outside of the arbitration field"
I send message with std id = 1 ( via another custom design board )
I set my mailbox configs :
ECanaMboxes.MBOX16.MSGID.all = 0x40000;
ECanaRegs.CANMD.bit.MD16 = 1;
ECanaRegs.CANME.bit.ME16 = 1;
(for my initializing and receive routine see : TIquestion.rarattachment)
but i cannot receive message..
I am waiting your help,
sorry for my bad English..
thanks.
Best regards from Türkiye.