Other Parts Discussed in Thread: TMS320C28346, TMS320C2834X
I would like to connect a 8MBit (512Kx16) flash to a TMS320C28346 device. For that reason I have downloaded the application spraaw0 which includes a sample schematic exacly for that case. If I compare that schematic to the XINTF reference guide (sprufn4a, chapter 2.7, please see picture) I think the sample schematic is wrong because address line XA0 (GPIO40) is not connected to the flash (like in a 32Bit data bus fashion). Now I'm a bit confused and don't know which of the two schematics is wrong.
Any ideas?
Thanks.