Other Parts Discussed in Thread: CONTROLSUITE
Hi I'm currently using the F28069 and HFI lib to implement IPD function,
I've apply for HFI.lib via local FAE
but I encounter a problem that the
HFI.lib won't work at FPU setting
is there floating point version of HFI.lib?
like the eSMO_float do.
"D:/ti/controlSUITE/libs/app_libs/motor_control/libs/HFI/v100/lib/HFI.lib<tr
ansition.obj>" specifies ISA revision "C2800", which is not compatible with
ISA revision "C28FPU32" specified in a previous file or on the command line
error: file