Hi,
I am converting my existing analog controlled full bridge DC-DC converter to digital by using TMS320F28027 and i have few queries on ADC configuration. In this analog control, the switching frequency was 165kHz and the output voltage ripple frequency was 330kHz (double the switching frequency). Now as the load increases the ripple voltage will increase and the sensed output voltage (scaled down to below 3.3V) to the ADC will vary accordingly.
1) How to configure the ADC channels for any DC-DC converter by considering the parameters like switching frequency & output ripple voltage.
2) How to configure the software filters (low pass or moving average) to filter out the noise in the sensed signal?
3) Are there any application notes on ADC configuration (C2000 controllers) for DC-DC converters.
Please suggest me.