I am simultaneously sampling two signals. SOCA goes low and I expect the sample and hold window to occur two adc cycles later and last for the period of time that I set(200ns). I see the wave forms on the scope and the sample hold period is in correct position to correctly sample the pulse, but it does not. It seems the sample hold window occurs some 700ns later than it should. I shut off all other ADC channels. Only two simultaneous samples triggered by a pwm compare and still 700ns later than the SOCA signal would indicate.
How can I accurately time my sample hold window? Other features claim 150ps resolution. This is way off.