This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C28X FPU FFT Library Phase Response



Hi,

I examined the fft library and examples for f28377x. "2837x_RFFT_Unaligned_ScaledMagnitude" and "2837x_WindowedRFFT" examples.

Both examples uses same input data. I understand that the magnitude outputs have different peak values because first example normalizes the data. But what about the phase output. Why are they look like so different? I plotted the input, magnitude and phase data to a excel file using "data_input.h", "data_output_1.h",  "data_output_2.h", "data_output_3.h" which are given in the example folder.Excel files are attached.

How can we interpret the result?

Regards,

FFT Excel.rar

  • I tested the software and understand the phase output. For example RFFTmagBuff[6] gives 3rd harmonic magnitude and RFFTphaseBuff[6] gives respective phase. I think other phase output values in the RFFTphaseBuff[] are irrelevant.