Hi,
There was a known IQmath issue about _IQNtoa function on IQmath v1.60. I'm using v1.5c instead of v1.6.
When the library wil be updated? If it will not how can I use v1.6 and pull the IQNtoa from v1.5c.
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
There was a known IQmath issue about _IQNtoa function on IQmath v1.60. I'm using v1.5c instead of v1.6.
When the library wil be updated? If it will not how can I use v1.6 and pull the IQNtoa from v1.5c.
Regards.
Hi,
CEM KOOSE said:When the library wil be updated? If it will not how can I use v1.6 and pull the IQNtoa from v1.5c.
What is the reason you want to use the above function from v15c? v160 has the same function too. Also, there's no issue with the function. Let us know why you feel so with a brief explanation.
Regards,
Gautam