This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSM with F28062F

Dear TI,


We are using the F28062F with CSM active.
like others on the support site, when the lock is active it won't work.
When you unlock it, it's ok.


When I read the other topics on the CSM you're mapping some functions to "rom_accessed_data" (RAMM0_M1)
Also .econst and .switch are mapped in RAMM0_M1

The problem is that it won't fit in RAMM0_M1 for my application. we use almost the complete resource of the chip.
A larger chip is also not possible (increase cost)


Is there another way to do it?


Best regards

Torius