Other Parts Discussed in Thread: TMS320F28027
Hello,
I am using TMS320F28027 LP for close loop control and PWM generation of H-bridge buck boost converter. It is a bit modified design of buck-boost having One Mosfet and One Diode in each leg.
Above image depicts the topology. With below ratings:
Vin: 19-100V
Vout: 72V
Power: 500W
Fsw: 75 kHz
I am using TMS320F28027 launchpad for close loop control and PWM generation. Both the pulses for top and bottom mosfet are same (ton and toff are same). The issue is, it works fine in complete range till 200 Ohm load, but as I reduce the load (increase the current level) PWM starts to ON/OFF frequently. This may be due to Noise, but controller pulses also turns on and off frequntly on low load. Currently I am only taking the output voltage feedback and changing the pulse width as the the feedback voltage. I seen and used some example and forum code and modified it a bit.
Can someone look at the code and let me know the issue with it..?
Thanks.
// Code for H bridge buck boost converter PWM
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#include "f2802x_common/include/adc.h"
#include "f2802x_common/include/clk.h"
#include "f2802x_common/include/flash.h"
#include "f2802x_common/include/gpio.h"
#include "f2802x_common/include/pie.h"
#include "f2802x_common/include/pll.h"
#include "f2802x_common/include/pwm.h"
#include "f2802x_common/include/wdog.h"
// Prototype statements for functions found within this file.
#define PWM1_TIMER_TBPRD 0x0190 //TBPRD = 400 == 75Khz
__interrupt void adc_isr(void);
void InitEPwm1(void);
// Global variables used in this example:
uint16_t LoopCount;
uint16_t ConversionCount;
//uint16_t V1, V2, V3;
uint16_t V4, V5, V6;
uint16_t Voltage1[20];
float Vout_count,Va,sum = 0;
float err_5, A_5=0,B_5=0, v_5=0, Vpi_5 = 0;
static float in_A = 0.0, k_5 = 0.0;
float V_duty;
float comp_value, Duty;
/*** PI controller **/
float Kp = 0.1; // [0] proportional gain
float Ki = 0.05; // [2] integral gain
float i10; // [4] I storage
float Umax = 0.99; // [6] upper saturation limit
float Umin = -0.99; // [8] lower saturation limit
float i6; // [A] saturation storage
ADC_Handle myAdc;
CLK_Handle myClk;
FLASH_Handle myFlash;
GPIO_Handle myGpio;
PIE_Handle myPie;
PWM_Handle myPwm1, myPwm2;
void main(void)
{
CPU_Handle myCpu;
PLL_Handle myPll;
WDOG_Handle myWDog;
// Initialize all the handles needed for this application
myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj));
myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj));
myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj));
myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj));
myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj));
myPwm2 = PWM_init((void *)PWM_ePWM2_BASE_ADDR, sizeof(PWM_Obj));
myPwm1 = PWM_init((void *)PWM_ePWM1_BASE_ADDR, sizeof(PWM_Obj));
myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));
// Perform basic system initialization
WDOG_disable(myWDog);
CLK_enableAdcClock(myClk);
(*Device_cal)();
//Select the internal oscillator 1 as the clock source
CLK_setOscSrc(myClk, CLK_OscSrc_Internal);
// Setup the PLL for x12 /2 which will yield 60Mhz = 10Mhz * 12 / 2
PLL_setup(myPll, PLL_Multiplier_12, PLL_DivideSelect_ClkIn_by_2);
// Disable the PIE and all interrupts
PIE_disable(myPie);
PIE_disableAllInts(myPie);
CPU_disableGlobalInts(myCpu);
CPU_clearIntFlags(myCpu);
// If running from flash copy RAM only functions to RAM
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
// Setup a debug vector table and enable the PIE
PIE_setDebugIntVectorTable(myPie);
PIE_enable(myPie);
PIE_registerPieIntHandler(myPie, PIE_GroupNumber_10, PIE_SubGroupNumber_1,
(intVec_t)&adc_isr);
InitEPwm1();
// Initialize the ADC
ADC_enableBandGap(myAdc);
ADC_enableRefBuffers(myAdc);
ADC_powerUp(myAdc);
ADC_enable(myAdc);
ADC_setVoltRefSrc(myAdc, ADC_VoltageRefSrc_Int);
// Enable ADCINT1 in PIE
PIE_enableAdcInt(myPie, ADC_IntNumber_1);
// Enable CPU Interrupt 1
CPU_enableInt(myCpu, CPU_IntNumber_10);
// Enable Global interrupt INTM
CPU_enableGlobalInts(myCpu);
// Enable Global real time interrupt DBGM
CPU_enableDebugInt(myCpu);
LoopCount = 0;
ConversionCount = 0;
ADC_setIntPulseGenMode(myAdc, ADC_IntPulseGenMode_Prior); //ADCINT1 trips after AdcResults latch
ADC_enableInt(myAdc, ADC_IntNumber_1); //Enabled ADCINT1
ADC_setIntMode(myAdc, ADC_IntNumber_1, ADC_IntMode_ClearFlag); //Disable ADCINT1 Continuous mode
ADC_setIntSrc(myAdc, ADC_IntNumber_1, ADC_IntSrc_EOC2); //setup EOC2 to trigger ADCINT1 to fire
ADC_setSocChanNumber (myAdc, ADC_SocNumber_0, ADC_SocChanNumber_A4); //set SOC0 channel select to ADCINA4
ADC_setSocChanNumber (myAdc, ADC_SocNumber_1, ADC_SocChanNumber_A4); //set SOC1 channel select to ADCINA4
ADC_setSocChanNumber (myAdc, ADC_SocNumber_2, ADC_SocChanNumber_A2); //set SOC2 channel select to ADCINA2
ADC_setSocTrigSrc(myAdc, ADC_SocNumber_0, ADC_SocTrigSrc_EPWM2_ADCSOCA); //set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1
ADC_setSocTrigSrc(myAdc, ADC_SocNumber_1, ADC_SocTrigSrc_EPWM2_ADCSOCA); //set SOC1 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1
ADC_setSocTrigSrc(myAdc, ADC_SocNumber_2, ADC_SocTrigSrc_EPWM2_ADCSOCA); //set SOC2 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1, then SOC2
ADC_setSocSampleWindow(myAdc, ADC_SocNumber_0, ADC_SocSampleWindow_12_cycles); //set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
ADC_setSocSampleWindow(myAdc, ADC_SocNumber_1, ADC_SocSampleWindow_12_cycles); //set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
ADC_setSocSampleWindow(myAdc, ADC_SocNumber_2, ADC_SocSampleWindow_12_cycles); //set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
// Enable PWM clock
CLK_enablePwmClock(myClk, PWM_Number_2);
// Setup PWM
PWM_enableSocAPulse(myPwm2); // Enable SOC on A group
PWM_setSocAPulseSrc(myPwm2, PWM_SocPulseSrc_CounterEqualCmpAIncr); // Select SOC from from CPMA on upcount
PWM_setSocAPeriod(myPwm2, PWM_SocPeriod_FirstEvent); // Generate pulse on 1st event
PWM_setCmpA(myPwm2, 0x0000); // Set compare A value
PWM_setPeriod(myPwm2, 0x05DC); // Period = 1388 for 5Khz Sampling Frequency
PWM_setCounterMode(myPwm2, PWM_CounterMode_Up); // count up and start
CLK_enableTbClockSync(myClk);
// Wait for ADC interrupt
for(;;)
{
PWM_setCmpA(myPwm1,Vpi_5); //TBPRD = 200
}
}
void InitEPwm1()
{
CLK_disableTbClockSync(myClk);
CLK_enablePwmClock(myClk, PWM_Number_1);
GPIO_setPullUp(myGpio, GPIO_Number_0, GPIO_PullUp_Disable);
GPIO_setPullUp(myGpio, GPIO_Number_1, GPIO_PullUp_Disable);
GPIO_setMode(myGpio, GPIO_Number_0, GPIO_0_Mode_EPWM1A);
GPIO_setMode(myGpio, GPIO_Number_1, GPIO_1_Mode_EPWM1B);
// Setup Sync
PWM_setSyncMode(myPwm1, PWM_SyncMode_EPWMxSYNC);
// PWM_setSyncMode(myPwm2, PWM_SyncMode_EPWMxSYNC);
// Allow each timer to be sync'ed
PWM_enableCounterLoad(myPwm1);
PWM_setPeriod(myPwm1, PWM1_TIMER_TBPRD);
PWM_setCounterMode(myPwm1, PWM_CounterMode_Up); // Count up
PWM_setIntMode(myPwm1, PWM_IntMode_CounterEqualZero); // Select INT on Zero event
PWM_enableInt(myPwm1); // Enable INT
PWM_setIntPeriod(myPwm1, PWM_IntPeriod_FirstEvent); // Generate INT on 1st event
PWM_setActionQual_Period_PwmA(myPwm1, PWM_ActionQual_Set);
PWM_setActionQual_CntUp_CmpA_PwmA(myPwm1, PWM_ActionQual_Clear);
PWM_setActionQual_Period_PwmB(myPwm1, PWM_ActionQual_Clear);
PWM_setActionQual_CntUp_CmpA_PwmB(myPwm1, PWM_ActionQual_Set);
CLK_enableTbClockSync(myClk);
}
__interrupt void adc_isr(void)
{
Voltage1[ConversionCount] = ADC_readResult(myAdc, ADC_ResultNumber_1);
sum += Voltage1[ConversionCount];
if(ConversionCount == 19)
{
Vout_count = sum/ConversionCount; // average count
Va = (Vout_count * 3.3)/(4096) ; // sensed voltage in 3.3V format
err_5 = 3.0 - Va;
A_5 = (err_5 * Kp); // kp multiplication
B_5 = (err_5 * Ki); // Ki multiplication
v_5 = k_5 + (B_5 + in_A);
if (v_5 >= 300) v_5 = 300; // maximum duty cycle limit
if (v_5 <= 00) v_5 = 00;
k_5 = v_5;
in_A = B_5;
Vpi_5 = A_5 + v_5;
if (Vpi_5 >= 300) Vpi_5 = 300;
if (Vpi_5 <= 01) Vpi_5 = 01; // minimum duty cycle limit
if (Va > 3.0) Vpi_5 = 01;
// if (err_5< 0) Vpi_5= 0;
ConversionCount = 0;
sum=0;
}
else ConversionCount++;
// Clear ADCINT1 flag reinitialize for next SOC
ADC_clearIntFlag(myAdc, ADC_IntNumber_1);
// Acknowledge interrupt to PIE
PIE_clearInt(myPie, PIE_GroupNumber_10);
// return;
}