Dear All,
We are working on F2837xD and we have designed our own board. I have made sample project to test Basic LED flashing and it is first test program I would be loading to my new board. Same is getting loaded properly on control card without any problem. I am facing some problem while loading on new board.
I get following message on CCS6.0 console window.
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_CPU1: File Loader: Data verification failed at address 0x00082000 Please verify target memory and memory map.
C28xx_CPU1: GEL: File: C:\Users\aakelkar\workspace_v6_0\f2837x_board\Debug\f2837x_board.out: a data verification error occurred, file load failed.
My boot load setting is load from flash.
I checked other details like, reset voltage, clock pulse etc. they are OK.
Since region 0x000820000 flash B region, I have also checked flash VDD pins. They are getting 3.3V.
Can any one give idea where could be problem? as I am using same .cmd file in both cases
Also in earlier versions of CCS to check Jtag connectivity, we had option of connect/disconnect processor . I am not sure how do I do it in CCS6. If I want to connect processor with out loading program , is there any way to do this?
not sure if it is possible?
regards
Abhijit Kelkar