Hi, I'm using TMDSHV1PHINVKIT. Now I've encountered a problem when I did the grid-tie experiment. I use a 380V/2A DC source to supply the inverter. When I connected it to grid, I can see the inverter under normal inverter mode from GUI then turn into Dc Bus Voltage Over quickly.
Grid side uses 220V/50Hz ac source, resistor load is 50 ohm.
I've tested Open loop and Closed loop without PLL, which works well.
problem:
1、Why this board works not with the actual grid?
2、wrong reason of Dc Bus Voltage Over? 380V/2A DC source is constant.
Does anyone know about this error? I need your help! Thank you!