This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PICCOLO + DRV8305 BOOSTERPACK STAND ALONE

Other Parts Discussed in Thread: DRV8305, MOTORWARE

Hi everybody,

I have the PICCOLO with the DRV8305 BOOSTERPACK and I want to run it stand alone with external pot for the speed rpm function. I have already set up "true" the variables:

gMotorVars.Flag_enableSys                         gMotorVars.Flag_Run_Identify

and the motor run fine stand alone with the default 100rpm speed, without the GUI.

Now I want to set up an ADC channel for the pot in order to control the speed.

Which variable controls the rpm speed?

Leo