Hi Champion,
F28377SPZP(100pin) package just has 15ch PWM, PWM2A, PWM2B, PWM3A, PWM6A, 6B, PWM7A, 7B, PWM8A, 8B, PWM9A, 9B, PWM10A,10B, PWM11A, 11B. PWM sync scheme in TRM as below:
my question is:
1. if I want to SYNC two independent group PWM, one need HRWPM function another is EPMW, each groupo include 3xPWM channel, as 100pin package, I can just choose PWM6-PWM8 as gproup1 for HRPWM and PWM9-PWM11 for Group2, but in the scheme, problem is PWM9 just can sync with PWM8 and cannot SYNC with PWM10 directly. So can I use PWM2 to SYNC PWM6 and PWM7, is it can be implement in 100 pin package becuause 100pin package donot have PWM1 and PWM4, so I am confuse this SYNC path is work?
2. In Revc TRM, there is a additional comment for SYNC is"make sure that the longest path does not exceed four ePWM/eCAP modules", what is means? If I use PWM1 SYN with PWM4 and PWM7 and PWM 11, ECAP1, there is 5 module SYNC, is it can implement? What's the reason to add this comment, can you give me some example maybe offend this rules?
Thanks!
BR
Joe