Other Parts Discussed in Thread: CONTROLSUITE
Hi Guys,
CCS v 6.1.3.0034 (compiler version = TI v15.12.1.LTS)
TMX320F28075 Control Card
control Suite v 3.4.0
Program : controlSUITE\device_support\F2807x\v200\F2807x_examples_Cpu1\epwm_trip_zone
Accordind to the Technical Reference Manual The GPAPUD is EALLOW protected.
Then in the following function from the above mentioned example program, why is there no EALLOW and EDIS for the GPAPUD ??
void InitTzGpio(void)
{
//
// For External Trigger, GPIO12 as the trigger for TripZone
//
GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; // Enable pull-up on GPIO12 (TZ1)
GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 3; // Asynch input GPIO12 (TZ1)
EALLOW;
InputXbarRegs.INPUT1SELECT = 12;
EDIS;
Also if I add EALLOW and EDIS then the trip zone interrupt doesn't work. Why so?
Thanks in advance.