For the F28027 launchpad, certain GPIOs on headers J6 and J2 appear to be linked together and I am wondering how I can access these pins individually. More specifically, GPIO 16 shares pin 7 of header J6 with GPIO 32, while GPIO 17 shares pin 8 of header J6 with GPIO 33 (a similar situation is seen on header J2). How can I separately access GPIOs 16, 17, 32, and 33?
Table 1 (of Ti SPRUHH2A) also shows pins 7 and 8 of header J6 have the GPIO's somehow linked together. It seems like there would be issues with setting GPIO 16 to be an input while GPIO 32 is an output. This is probably painfully obvious, but any help you can give would be greatly appreciated. Thanks.