Other Parts Discussed in Thread: TMS320F28075, TM4C123GH6PGE
Hi folks,
I am wondering if there are Piccolo (or indeed other TI devices) that allow multiple own addresses on I2C as a slave?
This is aside from the general broadcast address.
We are developing a prototype that uses a protocol that listens on several different multi-broadcast addresses as well as a specific slave address.
I am aware that some devices house 2 I2C modules which may solve the immediate problem, but these devices are very over-specced in all other areas and as such are considered too expensive. Such a solution that uses a second same I2C only offers one extra address. Our current requirement is at a very minimum one extra address but preferably two (in addition to the specific slave address and the general broadcast address).
Many thanks, T