Other Parts Discussed in Thread: CONTROLSUITE
Hi,
Customer wants to do a customized bootloader with SCI. In my point of view, there are two ways:
1) Prepare their own code to do the communication and Flash operation;
2) Call the internal whole bootloader from boot ROM SelectBootMode.
For the second way, is it possible? Where's the function point to call SCI bootloader?
For F28M35, customer did one CAN bootloader on M3. To reprogram C2000, do they need to write the code, or they can call some internal functions to program C2000?
Thanks a lot.
Br, Jordan