Other Parts Discussed in Thread: BOOSTXL-DRV8301
Hi, I had been running the labs on a smaller hard drive motor for testing with default system parameters starting with the motor ID lab2. Then I'd switched to a large Turnigy motor which has very low inductance but high speed and power (max power rating at 590W; max volt. at 15V) with the motor ID in lab2c. I had missed the user.h param, RES_EST_CURRENT, which led to the motor not spinning. I later corrected RES_EST_CURRENT which is all fine and it ID's and spins but what I'm worried about is when I had it at 1.0A (too low), towards the end of the run_identify it overloaded the power supply and produced a loud screech before run_identify switch to 0 (w/o error).
I'm wondering what would be causing this as I plan to hook up a much larger motor to the launchpad and don't want the same erratic power jump happening during the motor ID should I set the RES_EST_CURRENT too low.
I'm using the BoostXL-DRV8301 and Launchpad F28027F.
Thanks,
Scott