Other Parts Discussed in Thread: TIDA-00643, MOTORWARE, INSTASPINUNIVERSALGUI
I'm using a custom TIDA-00643 design and working through the steps as outlined in the tiduak1. I'm using a hobby motor that is very similar to the one in the tiduak1 appnote except that it is a 960kV motor with Rs=.07 & L=4.7uH The issue is that in lab05b is that since I don't know the inertia values of the motor and as a result can't calculate the Kp_spd/Ki_spd values, I attempt the trial and error method but I'm unable to find values of Kp_spd/Ki_spd which give the motor any sort of "spring" behavior. It just rotates with little to no resistance with no sort of spring back behavior.
Since this design uses a F2802xF device that means I can't use lab05c to identify the inertia of the motor correct? If that's the case would running lab05a and carrying out the procedure as described here be a better option?
And in general is it preferred to run these labs using the universal gui webapp or through CCS debug mode? I've tried both methods with lab05b.
Finally, I've been running these labs with the prop on as tiduak1 doesn't explicitly state whether the prop should be on/off for these labs. Is it recommended to have the prop on?
Best regards,
Shay