Hi,
I have a custom board based on the HVKit, with the difference being my own gate driver and FET's as opposed to an all-in-one module. The CPU is F28027F. We have had the motor running nicely on the HVKit, and have now transitioned to custom hardware.
I've been having a lot issues with the FET's switching. I have "fine tuned" my application and can achieve 200RPM, but the current waveforms are really bad, and I cannot understand "why" I would be seeing these sorts of waves.
I am taking my current measurements for each phase at the input points into the CPU.
My board is setup for 20A (+/-10A) same as HVKit.
At 100 RPM with VDC = 30V, I have the following Phase-U voltage (CH2) and Phase-U Current into the ADC (CH1).
And when zooming in on the rising edge of the phase voltage I note that the phase current is rail-to-rail. (indicating +/-10A)
Finally my design should run at a DC bus of > 200V. I'm just running it at low voltage for some basic tests.
If I run the design at VDC > 200V I have the top Phase U FET get super hot, while the rest are cool.
I could be looking at a hardware problem, some gate switching issue.
Can anyone lend some advice.
Thanks
Stomp!