Other Parts Discussed in Thread: TMS320F28PLC84
Project - PLC modem based on TMS320F28PLC84PNT, AFE031AIRGZR.
Net organisation is G3 Cenelec one master - many slaves. Master sends request, slaves reply.
1. In automatic mode modems self-determine the routes from master to slaves and vice versa. It takes up a lot of time, and this settings are lost when power is down.
Is it possible to save this setting somewhere in slaves and master memory to achive fast start?
2. Is it possible that this settings store in 24C1024 which is mentioned in reference guide, but not exist on demo-boards?
3. Is it possible to initialize modem with DBPSK modulation and then reconfigure it to more fast settings - even up to D8PSK - in case of good communication conditions?
Or modem do this automatically (switches to high speed settings in case of good communication conditions and switches back to low speed in case of noice environment).
4. Is it possible to build the network with 2000 nodes since joining process with 30 nodes takes up to 15 – 60 minutes (like it is mentioned in FAQ)? Or just not possible because lack of time?
http://processors.wiki.ti.com/index.php/Smart_Grid_PLC_FAQ#G3
5. Is it possible to build several independent subnet with different frequency band in one network? ( each subnet has own fixed frequency band).
6. If the modem has a power supply without galvanic isolation, could it be possible to use it without communication transformer? Does TI have a transformerless PLC reference design, can we get it?