Other Parts Discussed in Thread: DRV8301
Hello,
My setup is DRV8301 and LAUNCHXL-20869M.
I am trying to see the current that is going into the three phases of my motor.
I want to use the current patterns from all the three phases to control the position of the motor, as in get the total number of pulses from the motor and use that to set the position of my motor.
Is there a way that I can monitor these currents? or which points can i probe to observe these waveform on a scope ?
Is there such a variable that I can monitor that shows me the current being drawn by the driver? I cannot seem to find one in lab 05b.
Regards,
Rajan