Question in regards to the reference design of development kit for F28379.
1) In the datasheet, there are two power pins for F28379: VDDIO is for 3.3V digital I/O power pins while VDDA is for 3.3V analog power pins. In your reference design of ‘F2837x_180controlCARD_R1_3_SCH_02Oct2015.pdf”, the circuit is like this:
For VDDIO is connected to VDD_MCU_3V3; for VDDA is connected to VDDA_MCU_3V3. Why do we have to have a VDDA_MCU_3V3 for the analog power pin? Why not connect it directly to VDD_3V3?
I understand the reference design was trying to filter out the noises for VDDA_MCU_3V3, but for most design I saw, there was basically one VDD_3V3 for analog power and one VDD_MCU_3V3 for digital power pin. Is there a specific reason for adding additional filter to get the VDDA_MCU_3V3?
2) For U14 (IC_LDO_TPS62420DRC), the SW2 output is connected to 205k (R72) and 200k(R73) to get 1.2V. However, based on datasheet, the 1.2V is obtained by Vref * (1+R72/R73) with Vref = 0.6V. After the calculation, the Vout = 1.215V, not the expected 1.2V. If we change R72 to 200k, we will get the 1.2V. Why did the reference design chose R72 as 205k not 200k?