1. Do you have the ccs2.2 or ccs3.3 with Build Options of -m20, -g and -mw? I have both of them, but no these options. I'll appreciate you very much if you can e-mail me one or two with them.
2. Could you let me know the principle of ADC of DSP series '28x or help me to find relative reference? I only know it could work with 80ns min convention time under 25MHz ADC clock. It means for completing one convention only to need two ADC clock periods. I don' t know it is what kind of ADC?