This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
I am using f2806x instaspin-motion launchpad with boostxl-drv8301 REV B kit for my PMSM (45KW) motor.
Currently i am running that motor with my Power Supply (24V, 5A).
It is consuming 4A at 1200 rpm.
I need some suggestions-
1) Which can be the best driver pack to drive it with more rpm and power?
2) I am doing lab 10 where i didn't understand the concept of "trigger function" that is used to re-construct the current when narrow pulses are generated by the inverter. please elaborate this concept, how it is being used to for that purpose?
3) What is the concept of Ignore Shunt resistor?
Thanks.