Other Parts Discussed in Thread: CONTROLSUITE
Hi Guys,
CCS v 6.2(compiler version = TI v15.12.3.LTS)
TMX320F28075 Control Card
control Suite v 3.4.1
Example Program Used : ..\controlSUITE\device_support\F2807x\v200\F2807x_examples_Cpu1\sdfm_filters_sync_cpu
SDFM1 Settings:
- Only FILTER1 is enabled.
- SINC2, OSR_200, SHIFT_1_BITS
- AE_ENABLE
According to TRM the time for Data rate = 20us (@10MHz SDCLK). So I made a GPIO to toggle inside the SD1_ISR and got the following picture:
As you can see here, the time is not exactly 20us. Is this normal or am I doing something wrong?