Dear,
I checked around but did not find below parameters is used in anywhere in the PMSM3_3 project. Did I miss something or these parameters defined but NOT used at all:-
// This machine parameters are based on 1-hp PacSci PMSM motor
// Define the PMSM motor parameters
#define RS 0.9 // Stator resistance (ohm)
#define RR 0 // Rotor resistance (ohm)
#define LS 0.00435 // Stator inductance (H)
#define LR 0 // Rotor inductance (H)
#define LM 0 // Magnetizing inductance (H)
#define P 4 // Number of poles
// Define the base quantites
#define BASE_VOLTAGE 30 // Base peak phase voltage (volt)
#define BASE_CURRENT 5 // Base peak phase current (amp)
#define BASE_TORQUE 0.735105194 // Base torque (N.m)
#define BASE_FLUX 0.79616 // Base flux linkage (volt.sec/rad)