Other Parts Discussed in Thread: UNIFLASH, TMS320F28069
Hi,
I have a custom board with a F28069.
All is correctly working (CAN..).
There is one thing strange.
When I set a config with the PLL disable (using frequency of the external pin), the access to the board with UniFlash (CCS same thing) to erase the Flash banks is very slow compare to one if the board is loaded with a config with the PLL disable.
Do you have an idea?
I guess that Uniflash load a application that configures all the registers so this case should not happen..
Thanks in advance for your support
Regards,
Mathieu