Other Parts Discussed in Thread: PMP
Hi,
I have to convert 6-SPI clocked at 20Mhz. Each SPI are 32 bits. I need to have all those being converted to a single parallel port of 32bit (16 bit is still acceptable). So basically I have 6-SPI @ 20Mhz In and need to output 32 bits @ ~4Mhz or 16bits @ ~8Mhz. So the need is mostly in # of DMA, SPI, parrallel IO and clock speed.
I looked in microchip portfolio and they do have a few that seems to fit. But I would rather stick with TI if possible. But I don't seem to find what I want. The things becomes especially vagues for the parralel port part.
Ben