Other Parts Discussed in Thread: CONTROLSUITE
Hi,
Is it possible to flash this development board wireless ?
Usually there are some bootloaders that you need to flash first, and then you can flash HEX file wireless ?
Like using UART interface on board to the flashing ?
Of corse need also some PC SW that enables this interruct with the chip
If any one knows how to do so, please let me know.
I will use Bluetooth to UART module, so the wireless connection is with UART interface.
Usually the bootloader waits for few seconds, and if no respond it will jump to the memory start point of the program, and if there is a respond it will flash the chip
Thanks,
Roee