I do not use the controller module in InstaSPIN-FOC demos when using FAST to control my motor, like lab 11 without the controller module.
And Rs recalculation is not a need. Must the function EST_setFlag_enableRsRecalc( ) be called to disable Rs recalculation ?
If I do not call function EST_setFlag_enableRsRecalc( ) to disable Rs recalculation, what will happen ?
If offset recalculation is not a need. Must the function CTRL_setFlag_enableOffset( ) be called to disable offset recalculation ? (note that I do not use the controller module)