This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error 0x80000200/-1041

Sir

I have totally 5 Boards of my own design. Out of 5 boards 1 board is showing the problem as described below.

I checked all the signals at Emulator with working board and faulty board.

Everything is fine but when I connect to CCS i get error message as follows

Error connecting to the target:
Error 0x80000200/-1041
Fatal Error during: OCS, 
Device driver: Problem with the Emulation Controller.
It is recommended to RESET EMULATOR.  This will disconnect each 
target from the emulator.  The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.

I changed DSP in faulty board but it showing same problem.

 


If you guys find solution, kindly share details.

 

Thanks and Regards

Madhu Sagar M D