Hello
This post to signal a problem on CAN transciver ISO 1050 on board IDDK R2.2.
With the ControlCard F2837x, the lines CanRx and CanTx are inverted on C1 connector.
Pin 80 named "CAN-RX" is linked to the C1-CAN-TX line which is connected to Tx line of the CAN transceiver.
Same remark for the Pin 82 and the "CAN-TX"...
I made the test by invert these line and then, the CAN work with this modification!
Thank