Hi Champ,
Please let me confirm the ADC conversion time for F28075.
Pattern#1.
On the below case, please check if the conversion time is correct.
-ADC Clock : 30MHz
-Simultaneous Mode
-Number of ADC ch : 6ch
-ACQPS : 8
-Using the same trigger for SOC
Total conversion time = S/W time(9ADCCLK) + Conversion time (13*2ADCCLK) + S/W time(9-7ADCCLK) + Conversion time (13*2ADCCLK) + S/W time (9-7ADCCLK) + Conversion time (13*2ADCCLK) = 300ns+866.67ns+66.67ns+866.67ns+66.67ns+866.67ns = 3033.33ns
Pettern#2
In the below case, please check if the conversion time is correct.
And, Is both Sequential Mode and Simultaneous Mode used at the same time?
For example, ADCINA1, ADCINA3/ADCINAB3 pair, ADCINA7/ADCINB7 pair.
-ADC Clock : 30MHz
-ACQPS : 8
-ADCINA1、ADCINA3/ADCINB3 pair、ADCINA7/ADCINB7 pair
-Using the same trigger for SOC
Total conversion time = S/W time (9ADCCLK) + Conversion time (13*1ADCCLK) + S/W time (9-7ADCCLK) + Conversion time (13*2ADCCLK) + S/W time (9-7ADCCLK) + Conversion time (13*2ADCCLK) = 300ns+433.33ns+66.67ns+866.67ns+66.67ns+866.67ns = 2600ns
Regards,
Furuya