This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-HV-1PH-DCAC Single Phase Inverter Reference Design

Other Parts Discussed in Thread: TIDM-HV-1PH-DCAC, CONTROLSUITE

         Hi,
I am  searching  TIDM-HV-1PH-DCAC Single Phase Inverter Reference Design. I have found Altium and BOM files of the design from the design guide files. However; files only include main power card of the design. Gate drivers, control cards etc. files are not given in detail in the design guide. I am wondering do i have to make a custom design for them or are these TI products that can be ordered? Or are there Altium Files and BOM files of these control cards and gate drivers?
       Regards
       Alican

  • Alican,

    Please see in controlSUITE install: 

    C:\ti\controlSUITE\development_kits\HV_1PH_DCAC\v1_02_00_00\hardware\r3

    Gate driver file is also there but it's missing the altium project,

    C:\ti\controlSUITE\development_kits\HV_1PH_DCAC\v1_02_00_00\hardware\r3\IGBT Driver

    We will be doing a major update to this design end of Nov, if you can wait until then,,,

  • Thank you for your help,

    I have one more question, is it possible to use F28379D controlCARD as control card for this design? As I searched there is no big difference between F28379D controlCARD and TMDSDOCK28377D except position management control.

    Regards,
    Alican