This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301-HC-EVM J5 header ADC pins: Use as input?

Other Parts Discussed in Thread: CONTROLSUITE

Hi all

I am using the DRV8301-HC-EVM with F28069 MCU (CCS6).

Can I make use of the ADC pins on header J5 as inputs?

These pins are convetionally used for the three output phases on the board, but I am not making use of phase C and have two ADC inputs I'd like to sample.

Thanks

Stef