Other Parts Discussed in Thread: SFRA
I would like test SFRA functionality using my Experiments Kit
(Docking Station USB-EMU[R3] + F28035PNT control card Release1.0)
I'm trying to run the example project DPSWrkShpKit_SFRA_F28035.
I can buid and run the example project but the SFRA GUI is not finding any COM port using
SCI Connection Properties.
Could Someone help me to make the SCI communication work between SFRA and the experimenters kit work?
I set the control card SW2 BOOT according to the following:
Switch 1 ON (GPIO34)
Switch 2 OFF (TDO)
Best Regards