This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28075 Illegal Interrupt

Hi Team –

Posting this on behalf of a customer.

Currently using F28075. They currently have a RAM version code, which runs fine. The next step is to write the code to the on-chip flash, and run it from the flash.

When the code is written to flash, there are no errors during building. However, it is always stopping at illegal interrupt.

Can you please provide some comments to help move past this issue?

Thank you.