Other Parts Discussed in Thread: UNIFLASH, TMS320F2812
Hello,
We are working with the DSP TMS320F2812 and we develop for our product a serial software upload procedure. Therefore we program a Boot code into the TMS320F2812 and load the Application via a serial interface. Suddenly we cannot reprogram the TMS320F2812... The message in CCS Uniflash is:
[TIME] ERROR >> C28xx: Flash Programmer: Error erasing flash memory. Device is locked or not connected. Operation cancelled
[TIME] Unknown error
I have read a lot about the locked behaviour and therefore I used the function Program-Save/Export Memory in CCS Uniflash to read out the area 0x3F7FF8 - 0x3F7FFF and in this area are just Zeros. Additional I have read out the area 0x3D7BFC - 0x3F7FFF and this area are also filled with Zeros... So I guess this device is locked. In the Software we tried to load there are no Zeros, so I am a little bit confused.
Is there a possibility to unlock this TMS320F2812? Maybe to erase everything in the µC a kind of a full reset (Hardware reset)?
Setup:
CCS UniFlash 3.4.1.00012
JTAG-Emulator XDS510 USB
Thank you very much and my best regards,
Stefan